Solution
Bollard Pull Test
A bollard pull test is a procedure used in the maritime industry to measure the pulling or towing capability of a vessel. A force measurement system is needed to measure the vessel’s pulling power.
A bollard pull test is a procedure used in the maritime industry to measure the pulling or towing capability of a vessel. A force measurement system is needed to measure the vessel’s pulling power.
Interface’s WTSATL-JR Aluminum Compact Wireless Tension Load Link can be attached to the pulling line of the vessel and the bollard. Force results are wirelessly transmitted to the customer’s PC using the WTS-BS-4 USB Industrial Base Station, or to the WTS-BS-HA Handheld Display for single transmitters.
The customer determined the strength of the bollard when being pulled with Interface’s products.
Notifications